Other Parts Discussed in Thread: MSP430F6736A, , MSP-GANG, MSP430-FLASHER
Hi
I have a MSP-FET sitting betweena win10 PC and my custom board with a MSP430F6736A.
Connection is with a custom 8 wire ribbon cable, length 180mm.
The board is self powered.
An issue that has been annoying me for a long while is this:
The very fist time after reconnecting the FET to the PC & to the board, the FET loads my program without any problem.
The SECOND and SUBSEQUENT times i use the FET to load my program i get "Error connecting to the target: Unknown device".
Once that message appears, I then click on "Retry" and it loads normally!!
IF, however, i disconnect the FET from the PC (but keep the FET still connected to my powered board) PRIOR to loading my program, the FET loads my program EVERYTIME!
My questions are:
1. How can i get the FET to load my program everytime without having to disconnect it from the PC?
2. Why does this happen?
thanks in advance