This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/MSP432P401R: awake from LPM3 or 3.5, 4, 4.5 mode by using GPIO (button Interrupt)

Part Number: MSP432P401R

Tool/software: TI-RTOS

Hello, Guy

I need another help.

I posted "Interrupt Service Routine (ISR) never called in NO-RTOS based project ( after including TI-RTOS)"   (https://e2e.ti.com/support/microcontrollers/msp430/f/166/t/622382

In Opposite way, I tested that 

first of all, 

I created TI-RTOS based project ( empty_MSP_EXP432P401R_tirtos_ccs project from Resource View )

In this time, the problem is when the sensor enter deep sleep or shutdown mode (LPM 3, 3.5, 4, 4.5)

can awake it by GPIO interrupts  ?  I found example source code only using sleep mode (LPM0)  ( MSP432P401R Launchboard Red 2.X > TI Drivers > powersleep )

It shows that toggle between AM & LPM0 mode by using P1.1 button.

In Register Level Example, I found that button input is well at LPM3.5 mode

Please Some help me, plz

Thank you in advance.

**Attention** This is a public forum