Part Number: MSP432P401R
Today, all of a sudden, my MSP432 would not run its program without the Launchpad being plugged into the computer. Previously, I was always able to power it externally without any power from the debugger side of the Launchpad and the code would run perfectly. However, the MSP432 now waits in some sort of halted state until I plug the USB cable that runs from the debug side of the board into my computer. As I am not powering it through the debug side, I do not think this is a power issue. In addition, once the code starts after plugging the USB cable in, I can unplug the USB cable and the code will continue to run.
I have removed the 3V3 and 5V jumper pins from the debugger to the MSP432 side as I am powering the MPS432 from an eternal source. However, the debugger pins are still connected. It seems like the MSP432 is waiting in a halted state until it gets some sort of signal from the debugger. Is this possible?