This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm trying to configure my msp430 as an I2C slave and I want it to work the same way you would read a register out of any other slave. Usually by sending the device address, register address, issuing a restart, and then reading the data back. So far I'm able to write the register address and receive it in the MSP430, but after my master issues a restart and again sends the device address as a read, I do not get an ack.
Do I have to switch modes somewhere in order to send bytes out?
Here's my setup code:
void setup_slave_i2c(void){ // Configure GPIO P6SEL0 |= BIT4 | BIT5; P6SEL1 &= ~(BIT4 | BIT5); // Configure USCI_B2 for I2C mode UCB3CTLW0 = UCSWRST; // Software reset enabled UCB3CTLW0 |= UCMODE_3 | UCSYNC; // I2C mode, sync mode UCB3I2COA0 = 0x38 | UCOAEN; // own address is 0x48 + enable UCB3CTLW0 &= ~UCSWRST; // clear reset register UCB3IE |= UCRXIE | UCTXIE0 | UCSTPIE; // transmit,stop interrupt enable }
Here's my interrupt handler code:
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__) #pragma vector = EUSCI_B3_VECTOR __interrupt void USCI_B3_ISR(void) #elif defined(__GNUC__) void __attribute__ ((interrupt(EUSCI_B3_VECTOR))) USCI_B3_ISR (void) #else #error Compiler not supported! #endif { switch(__even_in_range(UCB3IV, USCI_I2C_UCBIT9IFG)) { case USCI_NONE: break; // Vector 0: No interrupts case USCI_I2C_UCALIFG: break; // Vector 2: ALIFG case USCI_I2C_UCNACKIFG: break; // Vector 4: NACKIFG case USCI_I2C_UCSTTIFG: UCB3IFG &= ~UCSTPIFG; /* Clear address and receive buffer */ __bic_SR_register_on_exit(LPM0_bits); break; // Vector 6: STTIFG case USCI_I2C_UCSTPIFG: break; // Vector 8: STPIFG case USCI_I2C_UCRXIFG3: break; // Vector 10: RXIFG3 case USCI_I2C_UCTXIFG3: break; // Vector 12: TXIFG3 case USCI_I2C_UCRXIFG2: break; // Vector 14: RXIFG2 case USCI_I2C_UCTXIFG2: break; // Vector 16: TXIFG2 case USCI_I2C_UCRXIFG1: break; // Vector 18: RXIFG1 case USCI_I2C_UCTXIFG1: break; // Vector 20: TXIFG1 case USCI_I2C_UCRXIFG0: // Vector 22: RXIFG0 UCB3IFG &= ~UCRXIFG; //clear rx ifg //UCB3CTLW0 |= UCTXSTP; // I2C stop condition //*RXData= UCB3RXBUF; *RXSlaveData = UCB3RXBUF; RXSlaveData++; //*RXData++; __bic_SR_register_on_exit(LPM0_bits); // Exit LPM0 break; case USCI_I2C_UCTXIFG0: // Vector 24: TXIFG0 UCB2TXBUF = 0xAA; __bic_SR_register_on_exit(LPM0_bits); // Exit LPM0 break; case USCI_I2C_UCBCNTIFG: break; // Vector 26: BCNTIFG case USCI_I2C_UCCLTOIFG: break; // Vector 28: clock low timeout case USCI_I2C_UCBIT9IFG: break; // Vector 30: 9th bit default: break; } }
What did I miss? Any advice is always appreciated.
Thank you
Thanks for posting the solution Eric, glad to see that you were able to figured it out. UCSTTIFG is defined as bit 2 of the UCB3IFG and is interrupt source 0x06 of the UCB3IV for eUSCI_B I2C operation. It should set when the I2C module detects a START condition together with its own address.
Ryan
**Attention** This is a public forum