This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430FR5994: LaunchPad needs to be reprogrammed

Part Number: MSP430FR5994
Other Parts Discussed in Thread: MSP-EXP430FR5994, , MSP-FET

Tool/software: Code Composer Studio

Dear Sirs:

      My launch pad bit the dust.  Its messages are:  Load Prog Error    then Load Fail !

So need to reprogram the ez-FET debugger on the launch pad.   Have been unable to find the proceedure and software.  

I also have an MSP-FET430UIF which I wired into the launchpad, bypassing the usb debugger on the launchpad (as shown on p41 of "MSP Debuggers".  Now when I try to download the software into the 430 chip nearly the same error message comes up:  Load Fail.

This seems to indicate that the 80 pin 430fr target chip has failed and not the onboard ezFET.  

Do you think this is true?

Thanks,

John

**Attention** This is a public forum