Hi,
I would like to use RTC module but I also have to wake up every second. Is it possible with RTC module?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I would like to use RTC module but I also have to wake up every second. Is it possible with RTC module?
Thanks.
The 4xx RTC module does not offer 1s interrupts, only 1m/1hr etc. And then only on full minute/hour.
You can set up the basic timer instead. It share the interrupt vector with the RTC anyway, so if the RTC is giving interrupts, the basic timer cannot and v.v.
With ACLK running on 32768Hz, 1s or 2s interrupts are easy with the basic timer. Select the ACLK/256 source and then set the interval with BTIP = fCLK2/128 (or /256 for 2s interval).
**Attention** This is a public forum