This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5659: LED to p2.0 instead of P1.0 on TS430PZ5x100 Eval board

Part Number: MSP430F5659
Other Parts Discussed in Thread: MSP430BT5190,

Has anyone noticed that the LED is connected to P2.0 instead of P1.0 on the 100-pin eval board? I ordered the 100 pin eval board for the 'F5xx family from Mouser, and got a TS430PZ5x100. On the schematic, it says the LED is connected to P1.0, but it is connected to pin 17 which is P2.0 on the F5xx processors. 

  • Table 1-1 of the Hardware Tools User's Guide (SLAU278) shows that the MSP-TS430PZ5x100 supports the MSP430F543x, MSP430BT5190, and MSP430SL5438A devices which have P1.0 at pin 17. I recommend the MSP-TS430PZ100USB for MSP430F5659 devices where P1.0 is located on pin 34 as expected.

    Regards,
    Ryan

**Attention** This is a public forum