Other Parts Discussed in Thread: MSP-EXP430FR5969
Hello!
I am new to msp430 technology and microcontroler programming. currently I am working on i2c but I am stuck with this problem. Please don't be harsh and correct me if i'm wrong but shoudn't __bis_SR_register(LPM3_bits + GIE); make the programm go into ISR? And what is the difference between LPM0 and LPM1(2,3,4)?
I added output commands so i could see in console where is my code getting stuck and it always stucks at shoudn't __bis_SR_register(LPM3_bits + GIE);
/*
* main.c
*/
#include <msp430.h>
#include <stdio.h>
unsigned char SlaveAddress = 0x76;
unsigned char TXByteCtr;
unsigned char RXByteCtr;
unsigned char *PTxData;
unsigned char *PRxData;
unsigned char RXData[6];
unsigned char TXDataArr[3];
void initI2C(void);
void RXdata(unsigned char reg_addr, unsigned char RX_byte);
void TXdata(unsigned char TX_byte);
void iic_TX(void);
void iic_RX(void);
void start_TX(void);
void start_RX(void);
void init_slave();
void read_slave();
int main(void)
{
WDTCTL = WDTPW | WDTHOLD;
//// I/O INIT
// Disable the GPIO power-on default high-impedance mode to activate
// previously configured port settings
PM5CTL0 &= ~LOCKLPM5;
P1SEL1 |= BIT6 | BIT7; // I2C pins
////
initI2C();
__bis_SR_register(GIE);
init_slave();
read_slave();
while(1)
{
//read_slave();
}
}
/////////////////// I2C B0///////////////////
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector = USCI_B0_VECTOR
__interrupt void USCI_B0_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(USCI_B0_VECTOR))) USCI_B0_ISR (void)
#else
#error Compiler not supported!
#endif
{
puts("interupt service routine entered\n");
switch(__even_in_range(UCB0IV,0x1E)) {
case 0x00: break; // Vector 0: No interrupts break;
case 0x02: break;
case 0x04:
UCB0CTLW0 |= UCTXSTT; //resend start if NACK
break; // Vector 4: NACKIFG break;
case 0x06: break; // Vector 6: STTIFG break;
case 0x08: break; // Vector 8: STPIFG break;
case 0x0a: break; // Vector 10: RXIFG3 break;
case 0x0c: break; // Vector 14: TXIFG3 break;
case 0x0e: break; // Vector 16: RXIFG2 break;
case 0x10: break; // Vector 18: TXIFG2 break;
case 0x12: break; // Vector 20: RXIFG1 break;
case 0x14: break; // Vector 22: TXIFG1 break;
case 0x16: // Vector 24: RXIFG0 break;
*PRxData++ = UCB0RXBUF; // Get RX data
RXByteCtr --;
if (RXByteCtr == 0) {
__delay_cycles(30);
UCB0CTLW1 |= UCSWACK;
UCB0CTLW0 |= UCTXACK;
UCB0CTLW0 |= UCTXSTP;
}
else {
UCB0IFG &= ~UCRXIFG0;
__bic_SR_register_on_exit(LPM3_bits);
}
break;
case 0x18:
if (TXByteCtr){ // Check TX byte counter
UCB0TXBUF = *PTxData++; // Load TX buffer
TXByteCtr--;
}
else {
UCB0CTLW0 |= UCTXSTP; // I2C stop condition
UCB0IFG &= ~UCTXIFG; // Clear USCI_B0 TX int flag
__bic_SR_register_on_exit(LPM3_bits);// Exit LPM0
}
break; // Vector 26: TXIFG0 break;
case 0x1A:
UCB0IFG &= ~UCBCNTIFG;
break; // Vector 28: BCNTIFG break;
case 0x1c: break; // Vector 30: clock low timeout break;
case 0x1e: break; // Vector 32: 9th bit break;
default: break;
}
}
void initI2C(void){
puts("initialising i2c");
UCB0CTLW0 |= UCSWRST; // put eUSCI_B in reset state
UCB0CTLW0 |= UCMODE_3 | UCMST | UCSSEL_2 | UCSYNC;// I2C mode, master mode, SMCLk /// + UCSSEL_2 | UCSYNC
UCB0CTLW1 |= UCASTP_2; //automatic stop generated
//after UCB0TBCNT is reached
UCB0BRW = 0x20; // 12
UCB0CTLW0 &=~ UCSWRST; //clear reset register
UCB0IE |= UCNACKIE | UCBCNTIE;
puts("initialising i2c successful");
}
void TXdata(unsigned char TX_byte) {
puts("calling iic_TX");
iic_TX();
puts("returned from iic_TX");
PTxData = (unsigned char *)&TXDataArr; // TX array start address
printf("PTxData = %d", TXDataArr[0]);
TXByteCtr = TX_byte; // Load TX byte counter
printf("TXByteCtr = %d\n",TX_byte);
puts("calling start_TX");
start_TX();
}
void iic_TX(void) {
puts("entered iic_TX \n");
printf("slave address = %d \n", SlaveAddress);
UCB0I2CSA = SlaveAddress;
puts("enabling tx interupt");
UCB0IE |= UCTXIE0; // Enable TX interrupt
puts("TX interupt enabled \n");
puts("exiting iic_TX\n");
}
void start_TX(void) {
puts("entered start_TX \n");
while (UCB0CTLW0 & UCTXSTP); // Ensure stop condition got sent
puts("stop condition sent \n");
puts("starting i2c TX\n");
UCB0CTLW0 |= UCTR + UCTXSTT; // I2C TX, start condition
puts("start condition met\n");
puts("entering interupt service routine\n");
__bis_SR_register(LPM3_bits + GIE); // Enter LPM0 w/ interrupts
puts("exiting start_TX\n");
}
void init_slave(){
puts("initialising sensor");
TXDataArr[0] = 0xF4;
TXDataArr[1] = BIT5 + BIT2 + BIT1;
TXdata(2);
puts("initialising sensor successful");
}
void read_slave(){
puts("reading data from sensor..");
RXdata(0xFA, 2);
puts("data read");
}