Part Number: MSP432P401M
Hello team,
Hope you are well. Would you be able make any recommendation for below requirements:
We are probably looking at Cortex M7/M4/M3 .
Low Power (Which would probably make our preference as M3/M4)
2 x sdio (mmc) interface (if this doesn’t exist then 1 maybe acceptable with another parallel bus)
It is desirable to have a direct DMA from SDIO / SDIO
SDIO rev 3.0 is desirable
>50 Mhz SDIO
SDR104 signaling
Support DDR50 signaling
Timer counter/capture module
1 16Bit parallel bus (32 width might be better) (2 bus interfaces might also be nice)
4 UART (2 might be ok, with FIFO would be good)
2x SPI (1 that can be service data via DMA)
>2MB ram (this could be external, see below, but for power/cost/space we might entertain something onboard)
Regards,
Randhir