This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-EXP430F5529LP: RXD powers 3.3V rail

Part Number: MSP-EXP430F5529LP

My EXP430F5529LP rev1.6 is connected to an USB port on PC, the 3V3 and 5V jumpers are disconnected, and the RXD jumper shows 2.7V. The problem is I can measure 2.1V on the 3.3V power rail coming from RXD jumper. It's normal? I couldn't find useful information in the slau533d.pdf. I'm just affraid of having an unexpected behavior when plug other devices.

  • Yes, it is "normal" but opinions differ as to whether it is a "bad thing". You are powering the device via the ESD diodes connected to RXD. In my opinion, since putting a voltage on a pin exceeds the Absolute Maximum rating, it should be verboten.

**Attention** This is a public forum