This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430F67791A: MSP430F67791A

Part Number: MSP430F67791A
Other Parts Discussed in Thread: TIDM-THREEPHASEMETER-F6779, TIDM-THDREADING, TIDM-3PHMETER-ROGOWSKI

Tool/software: Code Composer Studio

Dear All

I am trying to develop an 3 phase energy meter for one of our applications ,  i am using MSP490F67791A for the same ,  how ever i am unable to find the firmware or any other supporting libraries for the same can anybody share me the link for the same where i can get the library files so that i can start the development for the same 

  • Hello,

    I'm assuming that you're using the EVM430-F6779. There are several TI Designs based on this EVM. These include:

    • High Accuracy Three-Phase Electricity Meter with Tamper Detection (TIDM-THREEPHASEMETER-F6779)
    • Total Harmonic Distortion Measurement For Energy Monitoring Reference Design (TIDM-THDREADING)
    • Implementation of a 3-Phase Rogowski Coil Based Watt Hour Meter Reference Design (TIDM-3PHMETER-ROGOWSKI)

    On each of the TI Design product pages, there's a "Software" section where you can download the source code. You may be able to use links at the beginning of the User's Guides as well.

    Regards,

    James

    MSP Customer Applications

  • Hi James

    Thanks for replying i downloaded the same code which is IAR embedded work bench i would like to develop this product in CCS how ever i clearly went through the data sheet and app not SLAA577 i came across the formula to calculate the RMS voltage and RMS current i need to have a few clarity on the same formula in section 4.2.1.1 in which they have mentioned as

    vph(n) = Voltage sample at a sample instant n

    i dont understand this , is this an RAW ADC Result in hex

    i am starting from scratch for this project because it is for industrial application which has other parameters to be monitored and controlled
  • Hello,

    vijayanarayana ramamoorthy said:
    Thanks for replying i downloaded the same code which is IAR embedded work bench i would like to develop this product in CCS

    At this point, metrology code is not supported in CCS. Please see the links in the thread below.

    vijayanarayana ramamoorthy said:
    how ever i clearly went through the data sheet and app not SLAA577 i came across the formula to calculate the RMS voltage and RMS current i need to have a few clarity on the same formula in section 4.2.1.1 in which they have mentioned as

    vph(n) = Voltage sample at a sample instant n

    i dont understand this , is this an RAW ADC Result in hex

    i am starting from scratch for this project because it is for industrial application which has other parameters to be monitored and controlled

    Yes, Vph(n) represents a sample from a SD channel connected to a voltage channel. For the exact SD settings, you can find those by searching through the code/project.

    Regards,

    James

    MSP Customer Applications

**Attention** This is a public forum