Part Number: DRV8701EVM
Other Parts Discussed in Thread: MSP-FET
Tool/software: Code Composer Studio
hello,
i would like the DRV8701EVM with the MSP-FET debuggen and Code Composer Studio.
Which pins do I need to use? Do I need to install drivers?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DRV8701EVM
Other Parts Discussed in Thread: MSP-FET
Tool/software: Code Composer Studio
hello,
i would like the DRV8701EVM with the MSP-FET debuggen and Code Composer Studio.
Which pins do I need to use? Do I need to install drivers?
Hello,
JTAG pin 2 to board 3.3V_MCU, pin 8 to TEST, pin 1 to RESET, and pin 9 to GND. The drivers appear to already be installed. Be sure to make the connection wires as short as possible and post the specific error displayed if you are having connection issues.
Regards,
Ryan
**Attention** This is a public forum