Part Number: MSP430F5510
Hi,
I need to produce 8 PWMs in msp430f5510. I can implement 4 PWMs on one Timer (Timer A0) in the micro controller but now need 4 more PWM outputs (phase shifted by 180 degrees with reference to those produced in TimerA0). The duty cycle on the PWM needs to be varied in the code also. I can't seem to figure out a way in which I can start the Timer B by 180 degree delay. Also the frequency of the PWM is constant and around 150 KHz. Any help would be appreciated.
Thanks in advance!