This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR6989: MSPBSL_Scripter 3_02_01_00 Flash back issue

Part Number: MSP430FR6989
Other Parts Discussed in Thread: MSP-EXP430FR6989, MSP-FET, MSPBSL

hi,

i'm testing the BSL function of MSP430FR6989.

I'm using the MSP-EXP430FR6989 as the target platform.

and using the MSPBSL_Scripter(Windows version) as the host end, using MSP-FET be the bridge.

when i run the "BSL-Scripter.exe", no matter what commands i type, it always flash back immediately after press enter key.

need your help to see how to solve this problem, thank you.

  • Hi Erik,

    Make sure that jumper row J101 has been completely disconnected. Connect MSP-FET pin 1 to RST, pin2 to VCC, pin 7 to TEST, pin 9 to GND, pin 12 to P2.0, and pin 14 to P2.1. Use the proper commands as shown in SLAU655, using the examples provided in the software package. Provide images of the BSL-SCRIPTER command line error if the issue persists.

    Regards,
    Ryan

**Attention** This is a public forum