This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SIMPLELINK-SDK-BLUETOOTH-PLUGIN: version 0.0

Part Number: SIMPLELINK-SDK-BLUETOOTH-PLUGIN


Hi

I cannot import the project into Code compoer studio due to requirements for SIMPLELINK_MSP432_SDK_BLUETOOTH_PLUGIN v0.0.

Can some one please advise how/where I can download this version as the lowest downloadable is 1.0.

  • Hello,

    What procedure did you follow? Did you use the instructions here:
    software-dl.ti.com/.../users_guide_simplelink_msp432_sdk_plugin.html

    Best wishes
  • Hi ,

              Many thanks for your response, Unfortunately I am still experiencing the same issue when importing the project "blelock_MSP_EXP432P401R_tirtos_ccs" into Code Composer Studio. I have tried on both Ubuntu 14.04lts and windows 7 both 64bit machines. The error message is as follows.

           Error: Product 'com.ti. SIMPLELINK_MSP432_SDK_BLUETOOTH_PLUGIN' v0.0 is not currently installed and no compatible version is available. Please install this product or a compatible version.

     I have downloaded” ccs_setup_7.2.0.00013”, “simplelink_msp432p4_sdk_1_50_00_12" and "simplelink_msp432_sdk_bluetooth_plugin_1_20_00_42"  from your site and installing into "c:\ti" on the windows machine and similar equivalents onto the Linux box. The project files within the zip file ("tidcd85") has been unpacked into a project folder.

    Using the "Import CCS Projects... option under "Projects" tab within the Code Composer studio, I have selected the project above and attempted to load. Am I missing any additional installs?

    Regards

    Narendra

**Attention** This is a public forum