This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR6047: EVM communication issue

Expert 5080 points

Part Number: MSP430FR6047

Dear E2E Community,

My customer just get our EVM, but is not able to connect it through our USS GUI.

The driver is well set. But leds D201 and D202 remain off.

The customer loaded the project USSLib_GUI_Demo.projectspec (Version  01_30_00_04), through CCS:

 

The project can be compiled and loaded into the FR6047 through the USB.

 So the FR6047 and the related F5528 (to program it) work well (red section below); but the other F5528, related to the USB HID doesn't.

 

If S202 button is pushed and the EVM is plugged in, the MSP430 USB Firmware Upgrade software see the F5528 as expected:

 

After having loaded the HID Echo Firmware, the issue is still the same.

Any idea on how to process?

Can we provide the F5528 binary code of the EVM?

Regards,

**Attention** This is a public forum