Hi,
Can you help with below for a customer using the MSP430F247?
For device MSP430F247 the customer wants to know does the Errata SLAA423 apply to her design if her crystal is a 13 Mhz crystal and configuring LFXT1 in high frequency mode.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Can you help with below for a customer using the MSP430F247?
For device MSP430F247 the customer wants to know does the Errata SLAA423 apply to her design if her crystal is a 13 Mhz crystal and configuring LFXT1 in high frequency mode.
I don't know all the tricky behaviour to explain XOSC8 problem, but the short answer is no:)
There is other specification for high frequency range(13Mhz -> 3V min., use of external capacitor, duty cycle, ...) if he has a doubt about XT1 he cans test the crystal with XT2, the two oscillator should be the same
**Attention** This is a public forum