Part Number: MSP430G2553
Other Parts Discussed in Thread: AWR1443
Tool/software: Code Composer Studio
Hi,
I've connected an FMCW radar (AWR1443 BOOST) to an MSP430. The radar's is used for proximity sensing and sends a high signal (3.3V) to the msp430 to be read. The MSP430 turns off an LED when an object in 0.5m from the radar. The LED stays on otherwise. However, I was expecting the output of the GPIO pin of the MSP430 to be 3.3V when it's high. However, it's outputting a square wave with a max voltage of around 5V instead. I'm not sure why this is because without the radar connected, the GPIO outputs 3.3V as expected.
int main(void)
{
WDTCTL = WDTPW | WDTHOLD; // stop watchdog timer
P1DIR &=~ BIT1; // read from radar
P1DIR |= BIT2; // output to LED circuit
while(1){
if((P1IN && BIT1) == 0){
P1OUT |= BIT2; // turn on LED
}
else if((P1IN && BIT1) == 1)
{
P1OUT &=~ BIT2; // turn off LED
}
}
Any help would be appreciated