As far as I understand the "old" Filemaker program used for generating MSP430 Replicator code file
has been replaced by Srecord srec_cat.exe
The srec_cat program can be used to assemble the given input files into a single output file
I'm having trouble running Filemaker on Win7 64-bit and it would be nice to have an
optioanal program that could do a proper job formating the file for me
Hence, can srec_cat be used to generate the same output format as Filemaker.exe ?
Example output code file below
;Source File: C:\Replicator\code.txt
;Date: 11.10.2017
PUBLIC CodeArray
RSEG CODE
CodeArray
DW 0x0005 ; Number of Sections
DW 0xC000 ; Start address of section
DW 0x1125 ; Number of words in section
DW 0x120F, 0x120E, 0x120D, 0x120C, 0x120B, 0xB3D2, 0x002B, 0x2415
DW 0x42D2, 0x10FD, 0x0057, 0x42D2, 0x10FC, 0x0056, 0xC2F2, 0x0029
-
-
-
DW 0xFFFE ; Start address of section
DW 0x0001 ; Number of words in section
DW 0xC53A
end
Kind regards
Olav