Part Number: MSP432P401R
Other Parts Discussed in Thread: MSP432WARE
When building some code that includes the driverlib.h I am getting the following warning
../../driverlib/inc/msp_compatibility.h:145:41: warning: implicit declaration of function 'asm' [-Wimplicit-function-declaration]
#define __wfi() asm(" wfi")
^
../../driverlib/inc/msp_compatibility.h:146:41: note: in expansion of macro '__wfi'
#define __sleep() __wfi()
^
./src/sp_lpm.c:274:8: note: in expansion of macro '__sleep'
__sleep();
This only happens if I use the gcc compile flag -std=c99 . If I remove it, the warning goes away and the code builds fine, otherwise it fails to build.
My file includes the following:
#include <rom.h>
#include <rom_map.h>
#include <driverlib.h>
Is there any other header that should be included for this to work?
Thanks and regards,
Pedro