This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR4133: TI's version of RESET circuit

Part Number: MSP430FR4133
Other Parts Discussed in Thread: MSP-FET

I've seen several APP notes which implement a RESET circuit like this one:

What is the exact reason for doing this? Most data sheets talk only about
a pullup and a 1,1 nF (what a funny value) to GND if one is planning to
use SBW.
 
The 1,1 nF is because programmers can't drive higher capacitive loads.
But can they drive resistive loads like the R22 (which is effectively tied to
ground from an AC point of view in the design from above)?

I this case the R22 / C51 combo is probably there to add some additional
noise immunity. But can I be sure a programmer (like the MSP-FET) can
drive this thing through SBW?
 
Or is there a different reason for all this stuff?

**Attention** This is a public forum