I'm a big (amateur) fan of the MSP430 but I'd like a bit more RAM on the chip than the 128 bytes available. I see that TI are planning to launch G2xx chips with significantly more RAM and Flash ; I can't find a date for this beyond "mid 2011" - is there any more information when such will become available.
TIA.