This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5359: IQMath library function _FtoIQ

Part Number: MSP430F5359

I am trying to use IQmathLib for MSP430 and MSP432 version 01.10.00.05.   A call to the function _FtoIQ(0.5) results in an error Error[e46]: Undefined external "_FtoIQ" referred in ...

I did not find any reference to this function in the provided header file IQmathlib.h.

The documentation Page 24 lists this function as available.  The documentation also recommends that the function  _FtoIQ() be used instead of the function _IQ() which also can convert floating point numbers into fixed point format. (due to performance overhead) The function _IQ() compiles and works as expected.

I was wondering if the  _FtoIQ() function has been removed from the library and the documentation has not been updated?.

**Attention** This is a public forum