Part Number: MSP432P401R
Can i have example C code to initialize timer A2 to use a particular clock source (e.g ACLK, SMCLK) , since the data structure below does not include a clock source.
Timer_A_CaptureModeConfig captureModeConfig =
{
TIMER_A_CAPTURECOMPARE_REGISTER_4; // CC2 Register 4
TIMER_A_CAPTUREMODE_RISING_EDGE, //Rising Edge
TIMER_A_CAPTURE_INPUTSELECT_CCIxA, //CCIxA Input Select - Will use P6.7 which is TA2 CCR4 capture input CCI4A
TIMER_A_CAPTURE_SYNCHRONOUS, //Synchronized Capture
TIMER_A_CAPTURECOMPARE_INTERRUPT_ENABLE, //Enable interrupt
TIMER_A_OUTPUTMODE_OUTBITVALUE //Output bit value
};
The only capture example in the driverlib examples in the sdk i have installed, is in the 'msp432p4_sdk_1_50_00_12' example folder.
The example file is "timer_a_continous_vlo_period_capture.c" and the example just shows ACLK output on P4.2 which is connected to P2.4
in order to use TA0.1 to count the ACLK periods.
Thanks