Part Number: MSP430F5659
Hello TI Expert,
I have got a question from our customer who is facing the problem with MSP430F5659.
Would you please check the following phenomenon and answer the question?
[Phenomenon]
When MSP430F5969 is booted at low temperature like -25 degree C, they are seeing the problem that Fault Flag of XT2(12MHz) and XT1LF(32kHz) in UCSCTL7 cannot be clear and MSP430 cannot be booted up.
There are 13 units / 100 units that are not booted with being stopped in the following loop.
***************
do {
/* FLG Clear */
UCSCTL7 &= ~(XT2OFFG + XT1LFOFFG + XT1HFOFFG + DCOFFG);
/* FLG Clear */
SFRIFG1 &= ~OFIFG;
} while(SFRIFG1&OFIFG);
***************
After being powered on, XT1LF(32kHz) can start oscillating, then, CPU reset can be released for 1 sec and then XT2(12MHz) can start oscillating.
So it looks both crystals can be oscillating correctly.
There are 13 units that cannot be booted
- 8 units of 13 failure units
If they change the value of XT2DRIVE of UCSCTL6 from 01b -> 10b (so that the amplitude level of XT2 can be high), 8 sets of 13 sets can be booted up.
- Rest 5 units of 13 failure units
If they change the value of XT1DRIVE from 00b -> 11b (though they do not think it is related because it is Low Frequency clock but amplitude of 32kHz becomes a little high) and also change the value of XCAP from 10b to 11b, 4 sets can be booted up.
Regarding Last 1 unit, the amplitude level of XT1 out is about 190 -200mVp-p. If they ignore XT1LFOFFG loop, this unit can be booted without any problem.
[Question]
Our customer understands that some amplitude level of crystal is needed. But they cannot change the drive strength of XT1LF side.
So, if you have any required minimum amplitude level of crystal, would you please tell us how much level (what volts) is needed?
They think this problem is related with the amplitude level and as a result, Fault Flag is not clear.
Do you think there is any other reason? If you have any idea of other reasons, we would like you to give and comment.
They are using the following parts;
- 12MHz:NX2520SA 12MHz(NDK)+15pF
- 32kHz:NX1610SA 32.768kHz(NDK)+12pF
Regarding the load capacitors, they are using the value that matching is done by the crystal vendor.
Best Regards,
Nobu Arai