This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/MSP-EXP432P401R: Assembler Error Processor doesn't support ìt lt`in Thumb mode

Part Number: MSP-EXP432P401R


Tool/software: Linux

Hi,

I am a newbie having an embedded systems course in Coursera, and I am a bit late so the forum there is not active now.

We have to build an executable output for a given project using ubuntu OS and GNU make tool.

The following error message occur when trying to generate object file from the given c file.

I searched for this and I didn't find any info, about.

So any help would be greatly appreciated.

Thanks in advance.

ecee@embedded-vm:~/C1M2-Abubaker/src$ make build PLATFORM=MSP432
arm-none-eabi-gcc   -DMSP432 -I../include/common     -I../include/CMSIS -I../include/msp432   interrupts_msp432p401r_gcc.c -c 
/tmp/cc73SbT3.s: Assembler messages:
/tmp/cc73SbT3.s:54: Error: selected processor does not support `it lt' in Thumb mode
/tmp/cc73SbT3.s:55: Error: Thumb does not support conditional execution
Makefile:75: recipe for target 'interrupts_msp432p401r_gcc.o' failed
make: *** [interrupts_msp432p401r_gcc.o] Error 1

**Attention** This is a public forum