Part Number: MSP430FR6989
Other Parts Discussed in Thread: MSP430WARE
Tool/software: Code Composer Studio
Hi,
II am working on the project and we have the requirement of Flash integrity check at every start up
Below is the code and the project txt file
u
const uint32_t addr = 0x4400
uint32_t data_Calculate_CRC(uint32_t addr, uint32_t size )
{
CRCINIRES = 0xffff;
while (size != 0)
{
CRCDI_L = _data20_read_char(addr);
++addr;
--size;
}
return ((uint32_t)CRCRESR << 16) + ~CRCRESR;
}
My query: 4400 is the correct start address of flash memory?
what should be the size as txt will of 128 bytes
Seen many forum for the same topic but didnt get clear idea plz guide me for the same