This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432P401R: MSP432P401R

Part Number: MSP432P401R
Other Parts Discussed in Thread: CC2650

I am on TI Resource explorer attempting to do the CC2650 Module BoosterPack Out of the Box Demo. I have connected the CC2650 Booster pack to my MSP432P401R board. Once I click the button below to flash my MSP432 LaunchPad with the Project Zero software it loads slowly only before saying "Error configuring Debug Server: error= Operation was aborted". At first it also displayed that my USB was not showing up as well. I purchased a new USB cord to connect to my CPU from the MSP432P401R board, and that error went away. HELP PLEASE.  I also noticed that the board shown on screen was a RED MSP432P401R board with a 1.9 Rev. I have the BLACK MSP432P401R board with Rev of 1.0. Could that be the reason? 

**Attention** This is a public forum