Part Number: MSP430F5418A
Other Parts Discussed in Thread: MSP-GRLIB,
I am using the MSP-GRLIB with a MSP430F5418A attached to a Displaytech DT024DTFT QVGA display. All of the MSP-GRLIB functions work except the compressed images. The six images in the attached picture show the same image with 1, 4 and 8 bits per pixel uncompressed in the top row and 1, 4 and 8 bits per pixel compressed in the bottom row.
I do not believe this is caused by the MSP-GRLIB, but instead the MSP image reformer. Because, when I step thru the image function it writes the data from the image file correctly. Also I have manually corrected some of the artifacts in the image file and they display properly. Has anyone had this issue? Any feedback would be appreciated.
Thank you,
Darrell
Update: This could be related. I have found an image that the Image reformer will output a blank file for.
When the image reformer is set to 4 bits per pixel with compression the output is a blank file. The output is not blank for all the other settings.