This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FG6626: MSP430 with CC3210MOD

Part Number: MSP430FG6626
Other Parts Discussed in Thread: MSP430F5510, , CC3100, CC3120

Hi

I'm working on a wifi data collector, but until now I have been using the MSP430F5510 with a DeviceDrive WRF-01 WiFi Module. This has worked fine, but the WRF-01 does not support WPA2-Enterprise.

So I have to go back to the drawing board a little, so now I am looking at the CC3210MOD to use in conjuction with the MSP430FG6626 ( I need LCD, USB and 16Bit ADC)

There is lots of information the CC3210, but it's all about simplelink.  The simplelink looks like it only supports the MSP432, where the older CC3100 supported the MSP430.

Are you planning to port the simplelink for the CC3210MOD to the MSP430? 

Regards

Nick

**Attention** This is a public forum