Hi,I'm FAE of distributor in Japan.
Our customer would like to know behavior detail of PMM26.
They are checking PMM26 impact to their system they had developed before.
Their questions from about errata sheet(slaz251u.pdf) are bellow.
Q1)In case RST/NMI pin switch to NMI,does use case #2 happen?
"2) If RST pin is pulled low during write access to SVSMLCTL and only if the code that
checks for SVSMLDLYIFG==1 is implemented without a timeout. The device will be
stuck in the polling loop polling since SVSMLDLYIFG will never be cleared."
Q2) In case RST/NMI pin switch RST,does use case #2 make RST one time?
(Are Watchdog timer operating and it able to make reset?)
Q3) If Q1) is NO, why must we implement timeout as bellow?
"To prevent lock-up caused by use case #2 a timeout for the SVSMLDLYIFG flag check
should be implemented to 300us."
(Does this request come from different reason without PMM26?)
Regards,
Shinya Muramatsu.