Hello,
I am trying to link an EZ430-RF2500 AP with a custom board housing MSP430F1611 and a CC2500 + antenna (amongst other things).
After looking at the various examples (and trying some of them out) I came across the need of having a simpler way of adding the SimpliciTI stack to my application. Most of the examples contain a large number of files and configurations and the linker errors I get from trying to port this to the MSP430F1611 are hard to trace because they span over more linked source files.
Is there some bare bone project example for SimpliciTI already available that does not contain any bsp support at all?
Since an application to run on the MSP430F1611 already exists, it would be ideal to add SimpliciTI to that project while using the already existent defines.
I am also open to other suggestions.
UPDATE: I have managed to load up one of the examples from the SimpliciTI kit and create a new configuration in code composer to use with the custom board, however I have to edit the files I copied over from EZ430-RF board. Does anyone know a full list of things that need to be changed or maybe a template that allows me to build a board configuration just like in the TI examples? (the whole structure seems handy to have now that i've managed to understand how to use it)
Raziel