Part Number: MSP-EXP430FR5994
Other Parts Discussed in Thread: MSP430FR5994, MSP430WARE
Tool/software: Code Composer Studio
Hi everyone.
I have been playing with the msp430fr5994 for 2 months. I'm still learning C so sorry if my questions are obvious.
First of all i'm very confussed with the adc data. The values are (for expample) between -31472 and 22992. I can´t undestand it if the adc is 12 bits.
The second one is about the variable status wich is the return from de fft function. I can't si it on the watch window, why?
The last one is about the LEA memory. In the .map appears the length, and for the LEARAM is 0x00000ec8, 3784 bytes, why is not 4096? what is LEASTACK? if the real memory available is less than 4kb, which is the maximum fft possible?
Thank you.
Marcos.