Part Number: MSP430F5529
Other Parts Discussed in Thread: MSP-EXP430F5529LP
Tool/software: Code Composer Studio
I'm trying to program an MSP430F5529 on a custom PCB from the MSP-EXP430F5529LP launchpad. I am powering the MSP430 from the launchpad and jumping the JTAG pins from the launchpad programmer to the MSP430. When I try to debug in CCS, I get the error "Error connecting to the target: Unknown device."
Currently the PCB is only populated with the MSP430, power bypass capacitors, and VCORE capacitor. I am not using an external oscillator. The 47k pull-up and 1nF capacitor on the RST pin are connected externally, not on the PCB. The oscilloscope shows that the RST pin is not pulled low by the programmer and RST stays at 3.3v.
I have tried programming over SBW and have the same issue. Does anyone have any insight into this problem?
Thank you