Part Number: MSP430F67471A
Hello,
I have 3 questions.
1.I think "Icp,load" value(50uA) at the page op 51 in the datasheet is additionnaly flowed at AVCC pin or DVCC pin during Time to charge CLCD when discharged(500ms).
Is my understanding correct?
2.According to the datasheet page 30, it seems that the current consumption is larger when the charge pump is disabled than when the charge pump is enabled.
It seems that the consumption current is larger when the charge pump is enabled, why is it the result of the above?
3.If I want to compare the current consumption of the whole MCU with the data sheet, is it OK to use only the DVCC pin and AVcc pin to measure the pin?
Regards,
uchida-k