This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR4133: Header File Missing Port Definitions

Part Number: MSP430FR4133


Hello,

I am working on a Hall Sensor EVM that incorporates the MSP430FR4133.  On this EVM, I intend to use P8.2 with a push button.  In the process of trying to set up port 8 for my application, I noticed that the msp430fr4133.h header file is missing the  definitions for input, output, direction, resistor enable, selection, edge select, interrupt enable, and interrupt flag for ports 3 through 8.  Is there a newer header file available somewhere online?   If not, how should I set the definitions for P8IN, P8OUT, P8DIR, P8REN, P8SEL0, P8IE, and P8IFG?

**Attention** This is a public forum