Other Parts Discussed in Thread: MSP-GANG,
Hello,
We are using msp gang programmer for loading code file in the ic in production.
Production requirement is to save pass/fail log or resultfile using the serial no of each pcba that is programmed automatically through the software.
currently we are using script mode to load the code file into the ic. Read flash command is also not available in the instructions.
The Msp gang programmer for msp mcus .exe application doesnot allow this.
How can i achieve this?
How should i integrate this in the .exe file.? as the msp gang dlls cannot be imported into the visual studio application directly.