Dear TI team
I had designed PCB with MSP432 MCU, with 24MHz external crystal with 22pF decoupling capacitors., when i port the code for external crystal operation MCU stops.
the same code is working fine in launchpad in which 48mhz oscillator is used.
in my circuit all the components of VCC, Vcore are same as in launcpad except in place of 4.7uH, I had used 0E resistance. while in DCO operation it is working fine. external 32.768KHz is also working fine in LF pins.
Only IAR comiler is using.
can you expedite the issue.
Regards
Dharmesh Sachan