Part Number: MSP430FR2433
Other Parts Discussed in Thread: MSP-FET, ENERGIA
Tool/software: Linux
I got these 'promo' msp430fr2433 launchpads.
The doc says that it comes pre-flashed with "OutOfBox", and when I power up the board, red LED should flash approx. once in 5 seconds. But in fact, it flashes fast, several times per second, and this pattern does not change when I press J1 or J2 or both. And nothing comes over the backchannel UART.
I try to communicate with it via `mspdebug tilib` on Linux. Mspdebug behaves as if everything goes all right, and the red LED 101 on the probe lights up. I flash the supplied BlinkLED_MSP430FR2433.txt, and it reports no error, but there is no change in the blink pattern.
$ mspdebug tilib --allow-fw-update
MSPDebug version 0.22 - debugging tool for MSP430 MCUs
Copyright (C) 2009-2013 Daniel Beer <dlbeer@gmail.com>
This is free software; see the source for copying conditions. There is NO
warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.
MSP430_GetNumberOfUsbIfs
MSP430_GetNameOfUsbIf
Found FET: ttyACM0
MSP430_Initialize: ttyACM0
Firmware version is 4294967295
MSP430_VCC: 3000 mV
MSP430_OpenDevice
MSP430_GetFoundDevice
Device: (id = 0x0000)
0 breakpoints available
MSP430_EEM_Init
Chip ID data: 03 00 55
Available commands:
= erase isearch power save_raw simio
alias exit load prog set step
break fill load_raw read setbreak sym
cgraph gdb md regs setwatch verify
delbreak help mw reset setwatch_r verify_raw
dis hexout opt run setwatch_w
Available options:
color gdb_loop
enable_bsl_access gdbc_xfer_size
enable_locked_flash_access iradix
fet_block_size quiet
gdb_default_port
Type "help <topic>" for more information.
Use the "opt" command ("help opt") to set options.
Press Ctrl+D to quit.
(mspdebug) prog BlinkLED_MSP430FR2433.txt
Erasing...
Programming...
Writing 218 bytes at c400...
Writing 8 bytes at ff80...
Writing 38 bytes at ffda...
Done, 264 bytes total
(mspdebug) regs
( PC: 00000) ( R4: 00000) ( R8: 00000) (R12: 00000)
( SP: 00000) ( R5: 00000) ( R9: 00000) (R13: 00000)
( SR: 00000) ( R6: 00000) (R10: 00000) (R14: 00000)
( R3: 00000) ( R7: 00000) (R11: 00000) (R15: 00000)
0x0000:
00000: d0 38 JL 0x01a2
00002: ab 97 fc 7f CMP @R7, 0x7ffc(R11)
00006: 00 00 BRA @PC
00008: 01 00 MOVA @PC, SP
0000a: 00 00 BRA @PC
0000c: 00 00 BRA @PC
0000e: 00 00 BRA @PC
(mspdebug) regs
( PC: 00000) ( R4: 00010) ( R8: 00000) (R12: d368da60)
( SP: 00000) ( R5: 00000) ( R9: 00000) (R13: da4cce00)
( SR: 97ab33a8) ( R6: 00000) (R10: 00000) (R14: 00000)
( R3: 97ab3440) ( R7: 6884cb94) (R11: d368d560) (R15: 00010)
0x0000:
00000: d0 38 JL 0x01a2
00002: ab 97 fc 7f CMP @R7, 0x7ffc(R11)
00006: 00 00 BRA @PC
00008: 01 00 MOVA @PC, SP
0000a: 00 00 BRA @PC
0000c: 00 00 BRA @PC
0000e: 00 00 BRA @PC
(mspdebug) regs
( PC: 00000) ( R4: 00010) ( R8: 00000) (R12: d368da60)
( SP: 00000) ( R5: 00000) ( R9: 00000) (R13: da4cce00)
( SR: 97ab33a8) ( R6: 00000) (R10: 00000) (R14: 00000)
( R3: 97ab3440) ( R7: 6884cb94) (R11: d368d560) (R15: 00010)
0x0000:
00000: d0 38 JL 0x01a2
00002: ab 97 fc 7f CMP @R7, 0x7ffc(R11)
00006: 00 00 BRA @PC
00008: 01 00 MOVA @PC, SP
0000a: 00 00 BRA @PC
0000c: 00 00 BRA @PC
0000e: 00 00 BRA @PC
(mspdebug) run
Running. Press Ctrl+C to interrupt...
^C
( PC: 00000) ( R4: d368da60) ( R8: 97ab38d0) (R12: 00000)
( SP: 6884d065) ( R5: da4cce00) ( R9: 00001) (R13: 00000)
( SR: 46505845) ( R6: d368da60) (R10: d366ee00) (R14: 00002)
( R3: d368d560) ( R7: 00001) (R11: d324db8c) (R15: 00000)
0x0000:
00000: d0 38 JL 0x01a2
00002: ab 97 fc 7f CMP @R7, 0x7ffc(R11)
00006: 00 00 BRA @PC
00008: 01 00 MOVA @PC, SP
0000a: 00 00 BRA @PC
0000c: 00 00 BRA @PC
0000e: 00 00 BRA @PC
(mspdebug)
I got two boards and they behave the same way.
This all works with the old G2 launchpad and rf2500 driver.
Am I doing anything wrong? What's going on?
Thanks!