This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430 eZ430-RF2500 Sensor Monitor

Hi, I'm a noob with the MSP430 eZ430-RF2500 Development Tool. So I've made sure that Sensor Monitor project is compiled and linked OK - both AP and ED (it's the Sensor_Demo_AP_as_Data_Hub.eww  from CD, ver. 1.04, make+download using IAR Embedded Workbench ... hard to tell the version, the About is too long... drivers from 4/23/10 ), then  practiced with some other examples. Then I've tried to return to Sensor Monitor, and they don't  communicate. (Both AP and ED are alive, leds blinking, just don't communicate). What can be wrong? what do I have to check etc?

**Attention** This is a public forum