Part Number: MSP430F5308
Hi,
Brief question:
All the TI example code for UART operation used the external 32.768Khz crystal as the reference clock on XIN/XOUT.
It looks like from the Users Manual that I can use a 4Mhz crystal on XT2IN/XT2OUT to accomplish the same thing.
Is that correct for a baud rate is 115200?
Is there a downside to using XT2IN/XT2OUT and the higher frequency reference clock?
Thanks!
Blake