This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430F413: interrput - clock and UART communication

Hello, pleasee anyone help me.

I'm having trouble making two interrupts work correctly in my code

the first refers to a clock, and the second to my UART communication

independent the two work properly, however when enabling the two at the same time the UART communication stops working properly, sending any data.

follows part of the code:

int main (void){

hfsec = 0;
sec = 0;
min = 10;
hour = 21;

WDTCTL = WDTPW + WDTHOLD; // Watch Dog timer


FLL_CTL0 = XCAP18PF;                                        //0x0053 - FLL+ Control 0 = (0x30) - XIN Cap = XOUT Cap = 18pf
FLL_CTL1 = SCFQ_64K;                                        //fdco=64k - 0x0054 - FLL+ Control 1 =
SCFQCTL = 0x28 + 5;                                             //fLCD=fack/64 framing frequency~30hz - fMCLK = 2*fACLK
                                                                                 //Base timer 0.5sÖжÏÒ»´Î
IE2 |= 0x80;                                                              /* Interrupt Enable 2 */

LCDCTL = 0x5f;                                                   //s0-s11 fuctions as lcd segment lcdson=1 lcdon=1
P5SEL = 0xfc;                                                      //choose fuction:r13 r23 r33 com3.2.1

_BIS_SR(GIE); //equal to _EINT();*/
//_EINT();

UartConfig();

__bis_SR_register(GIE);

tx(0,"Diogel\r\n");

spi_setup();


while(1){                                             // main loop

lcd_clear();
varredura = kb_read();

savePass();

passRead();

if((KB_PORT_IN & LOG)==0){
log();                                                                         //here it returns me by serial communication the data of my memory


} // loop while (1)
} // função main



#pragma vector=BASICTIMER_VECTOR
//#pragma vector=TIMER0_A1_VECTOR
//#pragma vector=COMP_B_VECTOR
__interrupt void BT_ISR(void){
LPM3_EXIT;
hfsec++;
if(hfsec==2){
sec++;
hfsec=0;
}
// P6OUT^=LED0|LED1; //ledÃëµãÉÁ˸
// P6OUT^=LED0;

if(sec==60){
min++;
sec=0;
}

if(min==60){
hour++;
min=0;
}
if(hour==24){
hour=0;
}


SEC_H = tab[sec/10];
SEC_L = tab[sec%10];
MIN_H = tab[min/10];
MIN_L = tab[min%10];
HOUR_H = tab[hour/10];
HOUR_L = tab[hour%10];
}


// Timer A0 interrupt service routine
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=TIMER0_A0_VECTOR
__interrupt void Timer_A (void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(TIMER0_A0_VECTOR))) Timer_A (void)
#else
#error Compiler not supported!
#endif
{
CCR0 += Bitime; // Add Offset to CCR0

// RX
if (CCTL0 & CCIS0) // RX on CCI0B?
{
if( CCTL0 & CAP ) // Capture mode = start bit edge
{
CCTL0 &= ~ CAP; // Capture to compare mode
CCR0 += Bitime_5;
}
else
{
RXData = RXData >> 1;
if (CCTL0 & SCCI) // Get bit waiting in receive latch
RXData |= 0x80;
BitCntRX --; // All bits RXed?

if ( BitCntRX == 0) // se contador do RX zerar
//>>>>>>>>>> Decode of Received Byte Here <<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<
{
if (pBufRxGPRS>=TamBufRxGPRS-2){
pBufRxGPRS=0;
}


if (RXData == 13){
RXEnter = 1;
// RXDado = 0;
// RXDado = (BufRxGPRS[pBufRxGPRS-3]<<16) | (BufRxGPRS[pBufRxGPRS-2]<<8) | (BufRxGPRS[pBufRxGPRS-1]);
// pBufRxGPRS=0;
}


BufRxGPRS[pBufRxGPRS++]=RXData;

CCTL0 &= ~ CCIE; // All bits RXed, disable interrupt
__bic_SR_register_on_exit(CPUOFF); // Clear LPM0 bits from 0(SR)
}
//>>>>>>>>>> Decode of Received Byte Here <<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<
}
}
// TX
else
{
if ( BitCntTX == 0)
CCTL0 &= ~ CCIE; // All bits TXed, disable interrupt
else
{
CCTL0 |= OUTMOD2; // TX Space
if (TXData & 0x01)
CCTL0 &= ~ OUTMOD2; // TX Mark
TXData = TXData >> 1;
BitCntTX --;
}
}
}




  • Hello Thomas,

    Based on the code provided I assume you are encountering a race condition between the two interrupts. The BT ISR takes up too many cycles to service such that your TA ISR is delayed, causing UART communication failure. Either that or the LPM3 exit inside of your BT ISR interferes with your code flow. I recommend nesting interrupts, increases your MCLK frequency, or decreasing your UART baud rate. You might also consider upgrading to a device which provides a (e)USCI_A for a hardware UART solution.

    Regards,
    Ryan

**Attention** This is a public forum