This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F149: The chip is not programmed properly

Part Number: MSP430F149

 the chip run normal with the code loaded before , but now can not load the program, the programmer no problem,

  • Hi Jason,

    Did you check the VCC of the device to make sure it is powered properly? And also the JTAG connected well?

    BTW, which programmer you used? And which IED as well as the version?
  • Hi,

    thanks for your answer.

    this board can run normal with the code download before,so the VCC is OK.but now i can not download the code again.and i have two same board,the other board can download normal,so the debugger is ok. we can know that part of the chip is broken,or the Peripheral circuits that Associated with download  is broken.

    best regards

**Attention** This is a public forum