Part Number: MSP430FR2633
Other Parts Discussed in Thread: TM4C1294KCPDT,
Hello!
We are developing the lab device and now I'm looking for new keyboard design for it. The CapTIvate technology looks very useful here, as the device is small, and intended to be used in enviroments where some chemically active liquids can splash on keyboard, and also operator can have wet fingers, also in gloves.
The design of the device includes mainboard, which is attached directly to front panel, which is 1mm thick plastic. So I decided to print cap sensing buttons on the bottom side of the board, which is faced to front pannel. But, the board is rather small, and contains many components, including TM4C1294KCPDT MCU.
So the questions:
As the board is 4-layer, with power planes inside, what is the impact to sensors, if it is printed on the bottom side of the board and ground plane below? What is the impact, if some components, including 25-MHz crystall resonator or MCU or MSP430FR2633 itself is located on the top side of the board right above the sensors? Any other guidelines?
Thank you!