Part Number: MSP432P401R
Dear TI Experts,
One of my customer is developing charging center with MSP432, which can control the charging for several Power Bank with I2C bus. They find MSP432 will consume very big current ,around 800mA, when plugging I2C cable into MSP432 board sometimes, probability is about 20%. Under such abnormal status, all hardware function and software function of MSP432 is ok except the current in MSP432 will increase to 800mA, and the MCU get to hot. If they reset the MSP432, then current get back to the normal value and everything is fine. They suspect this issue is caused by ESD when plugging the cable, so they add ESD protector and small resistance on I2C bus, but seems not work. Do you have any suggestion about this issue? Thanks a lot.