Other Parts Discussed in Thread: TM4C1294NCPDT, TM4C129ENCPDT, CC3120,
Gentlemen,
I am usually active in the TM4C forum, although my first commercial projects were actually with MSP430's... It appears it is time to "come back" to the MSP community!
Several of our projects use TM4C1294NCPDT, and later, the crytpo equivalent TM4C129ENCPDT. Having trouble to purchase the 1294 chip this week, and having already heard of the new 120MHz MSP's, I decided to take a deeper look into the possibility.
Well, it seems that the IC's are EXACTLY the same product. They are pin to pin compatible, the muxing options for each pins are the same (as far as I had the patience to compare two datasheets), all peripherals are the same, memory identical... Given the fact that the MSP432 package is -40°C to +105°C, it actually relates to the T3 suffix on the TM4C device (the "best" out of the production line), and it is even a bit cheaper then their regular temp version.
Can anyone confirm that it is really the same thing? I've ordered a few samples, and also a launchpad, to give it a try, but apparently it is just a matter of compiling the project for the new family and VOILA! I wonder if the MSPWare syntax will be identical of the TivaWare? Any comments and suggestions are mostly welcome!
Regards
Bruno