What are the values of resistors R1,R2,R4,R6,R8,R9,R12 in above schematic?
can MSP430F5529 be programmed through usb using above board?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What are the values of resistors R1,R2,R4,R6,R8,R9,R12 in above schematic?
can MSP430F5529 be programmed through usb using above board?
Hi siddesh,
the values are 0 Ohm, SMD0805 (refer to the Bill of Material BOM in slac314b.zip (http://www.ti.com/litv/zip/slac314b).
Yes, you will be able to program the device via USB using this board (i.e. for firmware update in the field). For code development you should use the MSP-FET430UIF.
Rgds
aBUGSworstnightmare
**Attention** This is a public forum