Part Number: MSP430F5510
Hello,
I have two questions for MSP430F5510 RGC package.
1.
Are thermal pad and terminal pins on the exact same plane?
2.
I would like to know minimum requirement for percentage of exposed thermal pad joint area to PCB to keep thermal performance.
SLUA271 application note that the datasheet mentions at the package mechanical data page says like the below on P11.
“Typically, the solder-paste coverage is approximately 50% to 70% of the pad area (see Figure 11).”
From this descritpin, is it OK to think the minimum requirent is 50%?
Regards,
Oba