This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Programming an msp430f2272 with CCS4



Hi guys,

 

I was wondering if it is possible to program a MSP430 chip with CCS4 without having a project. Is there something like a hex file, so that I can just load it to program my chip. I already have a project made and it programs ok, I just need to send my "hex" file to somebody else so that they can program their board with my code. Is this possible with CCS4.

 

Thanks for any help

**Attention** This is a public forum