This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432P401R: Memory issue - #10099-D program will not fit into available memory msp432

Part Number: MSP432P401R

Hello Everyone,

I am working on MSP432p401R controller with BOOSTXL-EDUMKII booster pack and also interfacing audio boosterpack for an application.

I have some images to load on BOOSTXL-EDUMKII LCD and also some audio file to load for audio boosterpack .

in both the image and audio files the data are  char arrays.

so i am getting the error #10099-D program will not fit into available memory msp432.

It is taking the  .data section SRAM  which is 64k for it.

but i have Flash  256KB of which most of the part  is available .

How can i use the Flash to store my image arrays and audio array in it?

Thank you,

Sanath Rai

**Attention** This is a public forum